I/Q Out Block

This topic describes the settings accessed from the I/Q Out block. These settings allow you to configure the I/Q outputs of the instrument.

How to Configure and Use IQ Out

For M9484C, Option AN1 and DIQ are required.

For multi-channel instruments, Option AN1 and DIQ are available on Channel 1 only and the I/Q Out block is displayed for Channel 1 only (as shown in the screen below).

I/Q Output controls are based on the optional configuration of the instrument.

The GUI/SCPI descriptions for IQ Out settings are provided below.

DC Offset

Common Mode I Offset

Common Mode Q Offset

Diff Mode I Offset

Diff Mode Q Offset

Amplitude Control

Amplitude Control State

Amplitude Display Unit

I Amplitude

Q Amplitude

I Amplitude (RMS)

Q Amplitude (RMS)

I Amplitude (dBm)

Q Amplitude (dBm)

Endedness

I Amplitude Offset (dB)

Q Amplitude Offset (dB)

DC Offset

Common Mode I Offset

Requires Option AN1

This option is used to specify the common mode offset voltage routed to the external I+/I- output ports. The Common Mode Offset Voltage raises or lowers the voltage of the signal applied to the I+/I- output ports by the same value. A positive Common Mode Offset Voltage raises the voltage of the signal applied to external I+/I- output port above the baseline values, while a negative Common Mode Offset Voltage lowers the voltage of the signal applied to external I+/I- output port below the baseline values. For example, if the Common Mode Offset Voltage is +0.03 V, the baseline of both the external I+/I- outputs is shifted upward by 0.03 V. When no signal is applied (baseline condition), both outputs will measure +0.03 V.

The actual output voltage of an individual instrument may clip prior to achieving the minimum or maximum limit value. Verify your instrument is able to achieve your expected output prior to establishing your measurement procedure.

GUI Location

I/Q Out > Common Mode I Offset

SCPI Command

[:SOURce]:IQOut<channel>:IQADjustment:EXTernal:IOFFset <voltage>

[:SOURce]:IQOut<channel>:IQADjustment:EXTernal:IOFFset?

SCPI Example

IQO:IQAD:EXT:IOFF 5 mV

IQO:IQAD:EXT:IOFF?

Notes

For M9484C without Option AN1:

  • Attempting to change Common Mode I Offset raises the error 703, "Feature not supported; Common Mode I Offset unavailable, option AN1 is required."

Preset

0 V

State Saved

Yes

Min

-1.5 V

Max

1.5 V

Resolution

0.5 mV

Backwards Compatibility SCPI

N51xxB:

[:SOURce]:DM:IQADjustment:EXTernal:IOFFset

Backwards Compatibility Notes

For N51xxB:

Alias [:SOURce]:DM:IQADjustment:EXTernal:IOFFset to [:SOURce]:IQOut1:IQADjustment:EXTernal:IOFFset

Initial S/W Revision

A.01.00

Modified S/W Revision

A.10.00 - Min & Max range extended from -/+ 200 mV

A.11.50 - Updated for M9484C

A.20.00 - Added N51xxB Backwards Compatibility

Common Mode Q Offset

Requires Option AN1

This option is used to specify the common mode offset voltage signal routed to the external Q+/Q- output ports. The Common Mode Offset Voltage raises or lowers the voltage of a signal applied to the Q+/Q- output ports by the same value. A positive Common Mode Offset Voltage raises the voltage of the signal applied to external Q+/Q- output port above the baseline values, while a negative Common Mode Offset Voltage lowers the voltage of the signal applied to external Q+/Q- output port below the baseline values. For example, if the Common Mode Offset Voltage is 0.03 V, the voltage of the signal at both the external Q+/Q- outputs is increased by 0.03 V relative to the baseline.

The actual output voltage of an individual instrument may clip prior to achieving the minimum or maximum limit value. Verify your instrument is able to achieve your expected output prior to establishing your measurement procedure.

GUI Location

I/Q Out > Common Mode Q Offset

SCPI Command

[:SOURce]:IQOut<channel>:IQADjustment:EXTernal:QOFFset <voltage>

[:SOURce]:IQOut<channel>:IQADjustment:EXTernal:QOFFset?

SCPI Example

IQO:IQAD:EXT:QOFF 5 mV

IQO:IQAD:EXT:QOFF?

Notes

For M9484C without Option AN1:

  • Attempting to change Common Mode Q Offset raises the error 703, "Feature not supported; Common Mode Q Offset unavailable, option AN1 is required."

Preset

0 V

State Saved

Yes

Min

-1.5 V

Max

1.5 V

Resolution

0.5 mV

Backwards Compatibility SCPI

N51xxB:

[:SOURce]:DM:IQADjustment:EXTernal:QOFFset

Backwards Compatibility Notes

For N51xxB:

Alias [:SOURce]:DM:IQADjustment:EXTernal:QOFFset to [:SOURce]:IQOut1:IQADjustment:EXTernal:QOFFset

Initial S/W Revision

A.01.00

Modified S/W Revision

A.10.00 - Min & Max range extended from -/+ 200 mV

A.11.50 - Updated for M9484C

A.20.00 - Added N51xxB Backwards Compatibility

Diff Mode I Offset

Differential I output requires Option AN1 and Option DIQ.

Specifies a differential offset voltage for an in-phase (I) signal routed to the I+/I- output ports.

This option is used to specify the total differential offset voltage routed to the external I output port. The Offset Voltage offsets the signal routed to the external I output port by the value of this voltage. This is accomplished by adding half of the Offset Voltage to the signal applied to the external I+ output port and subtracting half of the Offset Voltage from the signal applied to the external I- output port. For example, if the desired I Offset Voltage is 0.05 volts, then 0.025 volts is added to the signal applied to the external I+ output port while 0.025 volts is subtracted from the signal applied to the external I- output port.

GUI Location

I/Q Out > Diff Mode I Offset

SCPI Command

[:SOURce]:IQOut<channel>:IQADjustment:EXTernal:DIOFfset <voltage>

[:SOURce]:IQOut<channel>:IQADjustment:EXTernal:DIOFfset?

SCPI Example

IQO:IQAD:EXT:DIOF 5 mV

IQO:IQAD:EXT:DIOF?

Notes

For M9484C without Option AN1 and Option DIQ

  • Attempting to change Diff Mode I Offset raises the error 703, "Feature not supported; Diff Mode I Offset unavailable, option AN1 and option DIQ are required."

Preset

0 V

State Saved

Yes

Min

-3 V

Max

3 V

Resolution

0.5 mV

Backwards Compatibility SCPI

N51xxB:

[:SOURce]:DM:IQADjustment:EXTernal:DIOFfset

Backwards Compatibility Notes

For N51xxB:

Alias [:SOURce]:DM:IQADjustment:EXTernal:DIOFfset to [:SOURce]:IQOut1:IQADjustment:EXTernal:DIOFfset

Initial S/W Revision

A.01.00

Modified S/W Revision

A.11.50 - Updated for M9484C

A.20.00 - Added N51xxB Backwards Compatibility

Diff Mode Q Offset

Differential I output requires Option AN1 and Option DIQ.

Specifies a differential offset voltage for a quadrature-phase (Q) signal routed to the Q+/Q- output ports.

This option is used to specify the total differential offset voltage routed to the external Q output port. The Offset Voltage offsets the signal routed to the external Q output port by the value of this voltage. This is accomplished by adding half of the Offset Voltage to the signal applied to the external Q+ output port and subtracting half of the Offset Voltage from the signal applied to the external Q- output port. For example, if the desired Q Offset Voltage is 0.05 volts, then 0.025 volts is added to the signal applied to the external Q+ output port and 0.025 volts is subtracted from the signal applied to the external Q- output port.

GUI Location

I/Q Out > Diff Mode Q Offset

SCPI Command

[:SOURce]:IQOut<channel>:IQADjustment:EXTernal:DQOFfset <voltage>

[:SOURce]:IQOut<channel>:IQADjustment:EXTernal:DQOFfset?

SCPI Example

IQO:IQAD:EXT:DQOF 5 mV

IQO:IQAD:EXT:DQOF?

Notes

For M9484C without Option AN1 and Option DIQ

  • Attempting to change Diff Mode Q Offset raises the error 703, "Feature not supported; Diff Mode Q Offset unavailable, option AN1 and option DIQ are required."

Preset

0 V

State Saved

Yes

Min

-3 V

Max

3 V

Resolution

0.5 mV

Backwards Compatibility SCPI

N51xxB:

[:SOURce]:DM:IQADjustment:EXTernal:DQOFfset

Backwards Compatibility Notes

For N51xxB:

  • Alias [:SOURce]:DM:IQADjustment:EXTernal:DQOFfset to [:SOURce]:IQOut1:IQADjustment:EXTernal:DQOFfset

  • Query returns the current diff mode Q offset for IQ output 1.

Initial S/W Revision

A.01.00

Modified S/W Revision

A.11.50 - Updated for M9484C

A.20.00 - Added N51xxB Backwards Compatibility

Amplitude Control

Requires Option AN1

The I+/I− and Q+/Q− output voltages can be adjusted while continuing to provide modulated RF output.

Amplitude Control State

Requires Option AN1

Remote command only.

Provided to allow programmatic compatibility with other Keysight Technologies signal generators. On this signal generator, Amplitude Control State is always enabled and cannot be disabled. This setting allows adjustment of I+/I- and Q+/Q- output voltages using the I Amplitude and Q Amplitude settings. These adjustments affect only the I/Q outputs and do not modify the RF output signal.

SCPI Command

[:SOURce]:IQOut<channel>:IQADjustment:EXTernal:AMPLitude[:STATe] ON|OFF|1|0

[:SOURce]:IQOut<channel>:IQADjustment:EXTernal:AMPLitude[:STATe]?

SCPI Example

IQO:IQAD:EXT:AMPL ON

IQO:IQAD:EXT:AMPL?

Notes

State is ON and not changeable, attempting to set to OFF raises error "703, Feature not supported; Amplitude Control State is always on for this instrument."

Preset

ON

State Saved

Yes

Initial S/W Revision

A.07.00

Modified S/W Revision

A.11.50 updated for M9484C

Amplitude Display Unit

Requires Option AN1

Selects the display unit used for I and Q Output Amplitude.

The units are related as follows:

where k = 1 for Single-Ended endedness and k = 2 for Differential endedness. This yields +3.01 dB when switching from Single-Ended to Differential for the same underlying signal amplitude.

GUI Location

I/Q Out > Amplitude Display Unit

SCPI Command

[:SOURce]:IQOut<channel>:IQADjustment:EXTernal:AMPLitude:UNIT VPEak|VRMS|DBM

[:SOURce]:IQOut<channel>:IQADjustment:EXTernal:AMPLitude:UNIT?

SCPI Example

IQO:IQAD:EXT:AMPL:UNIT VPE

IQO:IQAD:EXT:AMPL:UNIT?

Notes

This setting affects only the displayed amplitude values and does not alter the IQ output signal.

Preset

VPEak
Choices Vpeak| Vrms | dBm

State Saved

Yes

Initial S/W Revision

A.20.00

I Amplitude

Requires Option AN1

Sets the maximum voltage on I+ and I-. Maximum voltage occurs when waveform I data is 16-bit integer maximum (+32767), with minimum voltage occurring when I data is -32768. The voltage is for I into a 50 Ohm load.

GUI Location

I/Q Out > I Amplitude

SCPI Command

[:SOURce]:IQOut<channel>:IQADjustment:EXTernal:AMPLitude:I <voltage>

[:SOURce]:IQOut<channel>:IQADjustment:EXTernal:AMPLitude:I?

SCPI Example

IQO:IQAD:EXT:AMPL:I 1V

IQO:IQAD:EXT:AMPL:I?

Notes

For M9484C without Option AN1

  • Attempting to change I Amplitude raises the error 703, "Feature not supported; I Output Amplitude unavailable, option AN1 is required."

Couplings

This value, I Amplitude (RMS), and I Amplitude (dBm), all represent the same underlying I amplitude; setting any one recalculates the others.

See deriving equation in Amplitude Display Unit. The displayed value is also affected by Endedness and I Amplitude Offset (dB).

Preset

0

State Saved

Yes

Min

0 V

Max

- When Endedness is SINGle: 0.95 V

- When Endedness is DIFFerential: 1.9 V

Resolution

0.001

Initial S/W Revision

A.07.00

Modified S/W Revision

A.11.50 updated for M9484C

A.20.00 - Added dependency of max value on endedness

Q Amplitude

Requires Option AN1

Sets the maximum voltage on Q+ and Q-. Maximum voltage occurs when waveform Q data is 16-bit integer maximum (+32767), with minimum voltage occurring when Q data is -32768. The voltage is for Q into a 50 Ohm load.

GUI Location

I/Q Out > Q Amplitude

SCPI Command

[:SOURce]:IQOut<channel>:IQADjustment:EXTernal:AMPLitude:Q <voltage>

[:SOURce]:IQOut<channel>:IQADjustment:EXTernal:AMPLitude:Q?

SCPI Example

IQO:IQAD:EXT:AMPL:Q 1V

IQO:IQAD:EXT:AMPL:Q?

Notes

For M9484C without Option AN1

  • Attempting to change Q Amplitude raises the error 703, "Feature not supported; Q Output Amplitude unavailable, option AN1 is required."

Couplings

This value, Q Amplitude (RMS), and Q Amplitude (dBm), all represent the same underlying Q amplitude; setting any one recalculates the others.

See deriving equation in Amplitude Display Unit. The displayed value is also affected by Endedness and Q Amplitude Offset (dB).

Preset

0

State Saved

Yes

Min

0

Max

- When Endedness is SINGle: 0.95 V

- When Endedness is DIFFerential: 1.9 V

Resolution

0.001

Initial S/W Revision

A.07.00

Modified S/W Revision

A.11.50 updated for M9484C

A.20.00 - Added dependency of max value on endedness

I Amplitude (RMS)

Requires Option AN1

Sets the I output amplitude in Vrms. The value accounts for the endedness and I Amplitude Offset. See Endedness and I Amplitude Offset (dB).

GUI Location

I/Q Out > I Amplitude (RMS)

SCPI Command

[:SOURce]:IQOut<channel>:IQADjustment:EXTernal:AMPLitude:I:RMS <voltage>

[:SOURce]:IQOut<channel>:IQADjustment:EXTernal:AMPLitude:I:RMS?

SCPI Example

IQO:IQAD:EXT:AMPL:I:RMS 0.5

IQO:IQAD:EXT:AMPL:I:RMS?

Notes

For M9484C without Option AN1

  • Attempting to change I Output Amplitude (RMS) raises the error 703, "Feature not supported; I Output Amplitude (RMS) unavailable, option AN1 is required."

Couplings

This value, I Amplitude, and I Amplitude (dBm), all represent the same underlying I amplitude; setting any one recalculates the others. See deriving equation in Amplitude Display Unit. The displayed value is also affected by Endedness and I Amplitude Offset (dB).

Preset

0

State Saved

No

Min

0 V

Max

When Endedness is SINGle: 0.671 V

When Endedness is DIFFerential: 1.343 V

Resolution

0.001

Initial S/W Revision

A.20.00

Q Amplitude (RMS)

Requires Option AN1

Sets the Q output amplitude in Vrms. The value accounts for the endedness and I Amplitude Offset. See Endedness and Q Amplitude Offset (dB).

GUI Location

I/Q Out > Q Amplitude (RMS)

SCPI Command

[:SOURce]:IQOut<channel>:IQADjustment:EXTernal:AMPLitude:Q:RMS <voltage>

[:SOURce]:IQOut<channel>:IQADjustment:EXTernal:AMPLitude:Q:RMS?

SCPI Example

IQO:IQAD:EXT:AMPL:Q:RMS 0.5

IQO:IQAD:EXT:AMPL:Q:RMS?

Notes

For M9484C without Option AN1

  • Attempting to change Q Output Amplitude (RMS) raises the error 703, "Feature not supported; Q Output Amplitude (RMS) unavailable, option AN1 is required."

Couplings

This value, Q Amplitude, and Q Amplitude (dBm), all represent the same underlying Q amplitude; setting any one recalculates the others. See deriving equation in Amplitude Display Unit. The displayed value is also affected by Endedness and Q Amplitude Offset (dB).

Preset

0

State Saved

No

Min

0 V

Max

- When Endedness is SINGle: 0.671 V

- When Endedness is DIFFerential: 1.343 V

Resolution

0.001

Initial S/W Revision

A.20.00

I Amplitude (dBm)

Requires Option AN1

Sets the I output amplitude in dBm, referenced to a 50 Ω load. The value accounts for the endedness and I Amplitude Offset. See Endedness and I Amplitude Offset (dB).

GUI Location

I/Q Out > I Amplitude (dBm)

SCPI Command

[:SOURce]:IQOut<channel>:IQADjustment:EXTernal:AMPLitude:I:DBM <ampl>

[:SOURce]:IQOut<channel>:IQADjustment:EXTernal:AMPLitude:I:DBM?

SCPI Example

IQO:IQAD:EXT:AMPL:I:DBM -10

IQO:IQAD:EXT:AMPL:I:DBM?

Notes

For M9484C without Option AN1

  • Attempting to change I Output Amplitude (dBm) raises the error 703, "Feature not supported; I Output Amplitude (dBm) unavailable, option AN1 is required."

Couplings

This value, I Amplitude, and I Amplitude (RMS), all represent the same underlying I amplitude; setting any one recalculates the others. See deriving equation in Amplitude Display Unit. The displayed value is also affected by Endedness and I Amplitude Offset (dB).

Preset

-200 dBm

State Saved

No

Min

-200 dBm

Max

When Endedness is SINGle: 9.55 dBm

When Endedness is DIFFerential: 12.56 dBm

Resolution

0.001

Initial S/W Revision

A.20.00

Q Amplitude (dBm)

Requires Option AN1

Sets the Q output amplitude in dBm, referenced to a 50 Ω load. The value accounts for the endedness and Q Amplitude Offset. See Endedness and Q Amplitude Offset (dB).

GUI Location

I/Q Out > Q Amplitude (dBm)

SCPI Command

[:SOURce]:IQOut<channel>:IQADjustment:EXTernal:AMPLitude:Q:DBM <ampl>

[:SOURce]:IQOut<channel>:IQADjustment:EXTernal:AMPLitude:Q:DBM?

SCPI Example

IQO:IQAD:EXT:AMPL:Q:DBM -10

IQO:IQAD:EXT:AMPL:Q:DBM?

Notes

For M9484C without Option AN1

  • Attempting to change Q Output Amplitude (dBm) raises the error 703, "Feature not supported; Q Output Amplitude (dBm) unavailable, option AN1 is required."

Couplings

This value, Q Amplitude, and Q Amplitude (RMS), all represent the same underlying Q amplitude; setting any one recalculates the others. See deriving equation in Amplitude Display Unit. The displayed value is also affected by Endedness and Q Amplitude Offset (dB).

Preset

-200 dBm

State Saved

No

Min

-200 dBm

Max

When Endedness is SINGle: 9.55 dBm

When Endedness is DIFFerential: 12.56 dBm

Resolution

0.001

Initial S/W Revision

A.20.00

Endedness

Requires Option DIQ

Selects how the I/Q output amplitude voltage is displayed.

GUI Location

I/Q Out > Endedness

SCPI Command

[:SOURce]:IQOut<channel>:IQADjustment:EXTernal:AMPLitude:ENDedness SINGle|DIFFerential

[:SOURce]:IQOut<channel>:IQADjustment:EXTernal:AMPLitude:ENDedness?

SCPI Example

IQO:IQAD:EXT:AMPL:END DIFF

IQO:IQAD:EXT:AMPL:END?

Notes

This setting only affects the displayed amplitude values and does not alter the IQ output signal.

Preset

SINGle

Range Single-Ended|Differential

State Saved

Yes

Initial S/W Revision

A.20.00

I Amplitude Offset (dB)

Requires Option AN1

Provides a power offset value as a dB offset to the actual I output amplitude. This simulates a power level at a test point beyond the I+ and I- connectors without changing the actual output power. The offset value only affects the displayed amplitude setting. The offset is reflected in all I amplitude views (Vpeak, RMS, and dBm). See I Amplitude, I Amplitude (RMS), I Amplitude (dBm).

GUI Location

I/Q Out > I Amplitude Offset (dB)

SCPI Command

[:SOURce]:IQOut<channel>:IQADjustment:EXTernal:AMPLitude:OFFSet:I <rel_ampl>

[:SOURce]:IQOut<channel>:IQADjustment:EXTernal:AMPLitude:OFFSet:I?

SCPI Example

IQO:IQAD:EXT:AMPL:OFFS:I 3

IQO:IQAD:EXT:AMPL:OFFS:I?

Notes

For M9484C without Option AN1

  • Attempting to change I Amplitude Offset raises the error 703, "Feature not supported; I Amplitude Offset unavailable, option AN1 is required."

Preset

0 dB

State Saved

Yes

Min

-20 dB

Max

20 dB

Resolution 0.01 dB

Initial S/W Revision

A.20.00

Q Amplitude Offset (dB)

Requires Option AN1

Provides a power offset value as a dB offset to the actual Q output amplitude. This simulates a power level at a test point beyond the Q+ and Q- connectors without changing the actual output power. The offset value only affects the displayed amplitude setting. The offset is reflected in all Q amplitude views (Vpeak, RMS, and dBm). See Q Amplitude, Q Amplitude (RMS), Q Amplitude (dBm).

GUI Location

I/Q Out > Q Amplitude Offset (dB)

SCPI Command

[:SOURce]:IQOut<channel>:IQADjustment:EXTernal:AMPLitude:OFFSet:Q <rel_ampl>

[:SOURce]:IQOut<channel>:IQADjustment:EXTernal:AMPLitude:OFFSet:Q?

SCPI Example

IQO:IQAD:EXT:AMPL:OFFS:Q 3

IQO:IQAD:EXT:AMPL:OFFS:Q?

Notes

For M9484C without Option AN1

  • Attempting to change Q Amplitude Offset raises the error 703, "Feature not supported; Q Amplitude Offset unavailable, option AN1 is required."

Preset

0 dB

State Saved

Yes

Min

-20 dB

Max

20 dB

Resolution 0.01 dB

Initial S/W Revision

A.20.00